List of things to look for before placing an order for your design.
To get the best MachineBuilder experience, please consult the following minimum and recommended requirements.
Learn how to approach MachineBuilder like an expert. In this tutorial video, you will learn about the habits adopted by MachineBuilder professionals. 0:00 - Intro 0:47 - Starting a design 1:04 - Parts library discovery 2:07 - Inserting & connecting parts 2:57 - Snapping points 3:32 - Navigation compass 4:27 - Pre-orienting parts 4:52 - Compatible parts 5:21 - Sub-assemblies as parts 6:05 - Point to point connec...
How to use the Measurement Tools in MachineBuilder
How to connect and disconnect components in MachineBuilder
How to change the default navigation controls in MachineBuilder
Learn how to change your mouse navigation controls in MachineBuilder.
Learn how to resize extrusions in MachineBuilder.
How to use the Snapping Increment in MachineBuilder
Learn how to select multiple components in MachineBuilder.
Learn how to insert components in MachineBuilder.
How to navigate in 3D space in MachineBuilder
Take a tour of Vention’s Cloud-CAD platform, MachineBuilder. You’ll learn about different menus, part categories, and settings available to you as you design your machine. 0:14 - Opening MachineBuilder 0:38 - Parts menu 1:03 - Adding a part to our design 1:38 - Connecting parts 2:02 - View orientation 2:17 -Main menu 2:28 - Project action menu 2:41 - Quick actions 3:15 - Menu 4:08 - General design toolbar: l...
Learn how to use the Measurement Tools in MachineBuilder.
MachineBuilder is your solution for the rapid creation and design of factory equipment.
Learn the basics of navigating in 3D space in MachineBuilder. 0:00 - Intro 0:06 - Zoom 0:12 - Pan 0:17 - Rotate - Scroll wheel 0:25 - Rotate - Spacebar & Click 0:33 - Rotate - Nav Cube
How to insert components in MachinBuilder
In this how-to guide, we will cover basic, as well as more advanced, part insertion and connection functionalities of the Vention MachineBuilder platform.
Vention MachineBuilder does not provides 2D assembly drawings because they aren’t necessary in the context of Vention assemblies. All components are standard and modular to Vention’s library, so no custom manufacturing is needed for these components. Alternatively, all measurements you take in MachineBuilder will remain displayed until you delete them. This allows you to take screen captures of the front, top, side and...
Yes, you can import 3D files into MachineBuilder for all common CAD file formats, including SolidWorks, Catia, PTC Creo, Inventor, and more. Note that you can also export your model as a STEP file. The STEP files produced by MachineBuilder 3D are especially user-friendly because each part is stored as an individual body within the STEP file, and all part numbers are preserved.
Whether you want to see how your Vention Assembly is going to look in its environment or to design a custom part around your assembly, exporting a STEP file of your Vention Design is quick and simple.
Learn how to connect and disconnect parts in MachineBuilder.
Learn how to design using Vention's Modular Conveyor Ecosystem in MachineBuilder.
How to select multiple parts at once in MachineBuilder.
How to resize extrusions in MachineBuilder
Learn how to use the snapping increment in MachineBuilder.
Learn the basics as well as some tips and tricks on how to design a custom workstation using MachineBuilder.
Learn how to design a gantry robot within MachineBuilder Here are the list of resources for your reference: Design Link Selecting a linear actuator Configuration Assistant Tutoriak Linear guide datasheet Forum 0:00 - Intro 0:45 - Designing a Two-Axis System 2:13 - Designing a Rigid Base Frame 3:39 - Designing a Three-Axis System 6:43 - Additional Hardware
Learn how to design a belt conveyor within MachineBuilder Here are the list of resources for your reference: Conveyor Datasheet Designing with T-Slot Aluminum Extrusions 0:00 - Intro 0:42 - Getting Started 1:02 - Add Conveyor 1:59 - Design Base Frame 3:00 - Add Automation
Learn how to import your own 3D parts into MachineBuilder. 0:00 Intro 0:25 Import custom part 2:40 Connect imported parts 3:45 Export a design 4:02 Insert component
Take a tour of Vention MachineBuilder to discover how to add custom panels to your design. Great for , great for workstations and custom equipment. You will learn about the various panel materials, generating the panel, as well as the positioning and the fastening options. 0:00 - Intro 0:17 - Selecting panel materials 1:38 - Outside panels and retaining options 2:24 - Inside panels and retaining options 2:46...
Navigate to Designs in the side menu of your dashboard. Click the Edit menu or icon on the far right. In the list of options, choose Edit Properties. When the pop-up appears, click on the Privacy tab and change Privacy to public. Alternatively, open your design in MachineBuilder and click the Share button located top right of the toolbar and click on Share with community . Follow the step-by-step...
Whether you want to validate your robot’s workspace or visualize all connection points of your equipment to your assembly, inserting your own 3D models into your Vention design is fast and easy.
The group/ungroup feature in the MachineBuilder platform was designed to support the creation of logical groups, which can easily be moved, copied and re-used within an assembly.
The configuration assistant provides users with step-by-step instructions for designing with complex components. Configure a fully functional actuator with various guidance systems, gantry plates, sensors and motors. Settings (0:27) Getting started (0:44) Configuration assistant (0:54) Navigation compass (1:19) Custom part selection (1:36) Autocomplete (2:04) Reconfigure (2:23)
In this tutorial, you’ll learn how to add a robot to your design, position it within your robot cell, and how to simulate a robot reach study to validate your design manually. 0:00 Intro 0:21 Adding a robot 0:38 Position your robot
Learn how to design with our light-duty extrusions and present the set of hardware required to integrate them into our modular hardware platform. 0:00 - Intro 0:28 - Light-duty extrusion 0:34 - Resize extrusions 0:40 - Frame connectors 0:57 - Light-duty to standard extrusion connectors 1:12 - Associated fasteners
Learn a series of shortcuts for part placement, part selection, grouping, and view options in MachineBuilder. 0:00 - Intro 0:20 - Part placement shortcut 0:40 - Undo-Redo 0:51 - Part selection 1:29 - Group and ungroup parts 2:15 - Copy and paste 2:47 - View/Rotation shortcuts
Learn the basics of MachineBuilder to get you started on designing your Vention structures and machines. 0:00 - Intro 0:21 - Parts library 0:57 - Adding parts to your design 1:05 - Resize single extrusion 1:17 - Connecting parts 1:43 - Re-insert parts 2:35 - Resize multiple extrusions 3:17 - Sliding parts 3:27 - Design increments 3:45 - Point to point connection 4:12 - Connection checker
The Momentary Pushbutton Module extends MachineMotion 2’s functionality with two momentary pushbuttons. This plug-and-play module only requires a single connection to the MachineMotion 2 controller.
This document serves as an installation guide as well as a design guide for the cable management ecosystem.
After completing your design, you may want to share the design with your team members, colleagues, friends, or clients. You will have various visibility options you may choose from.
This how-to-guide covers the use of Vention’s MachineLogic, an easy-to-use visual sequence editor that can be accessed directly from MachineBuilder.
Ready to assemble your first Vention design? This guide presents all the tools and resources available to you for a successful assembly from start to finish.
A comprehensive guide to selecting the right Vention linear axis actuator for your application.
Learn how to check out your very own designs from Vention. You'll learn how to update your corporate account information, check out using your cart or a PDF quote as well as how to get updates on your order. 0:00 - Intro 0:21 - Check Corporate Account Information 0:45 - Edit Corporate Account Information 1:18 - Cart Checkout 2:08 - Methods of Payment 2:53 - PDF Quotes 2:58 - Generate PDF Quote: MachineBuilder 3:09 ...
MachineLogic enables you to program your robots online in our code-free environment. Perfect for Machine Tending cells. Developed automation sequences can be fully simulated inside MachineBuilder and then accessed directly from the MachineMotion pendant. Here are the list of resources for your reference: Design Link 0:00 - Intro 1:08 - Configure your robot 1:33 - Program - create your application 2:20 - Add ...
Include at least one MachineMotion controller, an actuator with end-stop sensors and gantry plate or a pneumatic actuator in MachineBuilder to be able to simulate in MachineLogic.
Learn how to configure Vention’s linear actuators, program by adding motion commands in MachineLogic, and simulate a sequence in MachineBuilder Check our Automated Applications page for inspiration on where to get started Here are the list of resources for your reference: Selecting a Linear Axis Actuator User Forum Design Link Configuration Assistant Tutorial 0:00 - Intro 0:20 - Getting Started 1:08 - Configu...
MachineMotion is a plug-and-play, single-box motion controller that includes everything you need for motion control: motor drives, power supply, control card, safety relay, and more. These components are all integrated into a complete system providing a true plug-and-play experience. For example, motors and sensors come pre-wired with connectors and plug directly into the MachineMotion controller box. In s...
Vention’s Safety Enclosure system features all the necessary components to deploy a complete safety fencing system or robot cell that integrates directly with the MachineMotion’s safety rated input.
Get quick answers to your questions by browsing our user forum or contacting technical support.