For manufacturers in food, beverage, pharmaceutical, and consumer goods, the end of the production line is often where efficiency bottlenecks surface first. Increased demand for faster production and persistent labor shortages, combined with continued reliance on manual labor for case packing and palletizing, drives higher turnover, ergonomic risk, and inconsistent throughput.
At Interpack 2026 in Düsseldorf, Vention and Universal Robots demonstrated a different approach to end-of-line automation through live, production-grade packaging cells.
Catch up on the key moments from the show and see how complete end-of-line systems can be deployed quickly on a unified automation platform, without complex programming or fragmented integration.
The Next Generation Rapid Series Palletizer Makes Its European Debut
The headline moment of the show was the European debut of Vention’s Next Generation Rapid Series Palletizer, powered by a Universal Robots UR20 collaborative robot. Built for the final stage of end-of-line packaging automation, the Next Generation Rapid Series handles the transition from packaged cases to pallet-ready shipments in a format that deploys faster and adapts more easily than traditional palletizing equipment.
![]()
Visitors to Vention’s booth had the chance to see the system running live palletizing cycles: cases moving from Vention’s new modular roller conveyor directly into a compact palletizing cell, with the UR20 efficiently stacking multiple SKU formats.
Alongside the live cell, visitors could also see Vention’s RemoteView displaying a live feed of the palletizer in real time, demonstrating how machine visibility works in practice with Vention’s platform.
The response on the show floor reflected a wider shift underway in European manufacturing. Teams that have long relied on manual palletizing are actively looking for a faster path to automation, and the Next Generation Rapid Series Palletizer, running live with a UR20 in a compact modular cell, gave them a concrete example of what that looks like in practice.
Discover the Rapid Series Palletizer
Flexible Robotic Case Packing for High-Mix Production
Case packing is often treated as a solved problem, until SKU complexity and the need for consistent quality makes it anything but. Traditional case packing equipment tends to be format-specific, which means every new product variant introduces a changeover challenge or a new machine entirely.
The live case packing demo at Vention’s booth demonstrated an effective solution to this challenge.
![]()
A UR10e collaborative robot handled product loading into shipping cases across multiple SKU configurations, in a compact cell built for operations that need flexibility without a large footprint. For attendees managing growing SKU complexity, it was a practical illustration of how robotic case packing can relieve bottlenecks, streamline packaging operations, and be delivered in just 12 weeks.
Live MachineAnalytics data running alongside the cell showcased how performance metrics are tracked in real time, making it easy to monitor throughput and identify issues without relying on manual observation.
A Fully Integrated Conveyor Ecosystem
Connecting case packing and palletizing is the conveying layer, and at Interpack, that piece of the line was running on Vention’s newly expanded conveyor ecosystem, announced just days before the show opened.
The expanded offering includes modular O-Ring and Poly-V roller conveyors, Vention-designed motors, and a complete suite of add-ons, all controlled through MachineMotion AI and programmed via MachineLogic. That means the same controller and software environment that runs the palletizer and case packing cell also manages product flow between them, eliminating the need for separate PLC programming or third-party conveyor integration.
For packaging manufacturers, the practical implication is significant. Conveyor systems that traditionally required custom engineering to connect with upstream and downstream equipment can now be configured, sequenced, and reconfigured directly by operators, without specialized support.
One Platform for the Full End-of-Line Packaging Journey
Together, the demos at Interpack illustrated how the full end-of-line packaging sequence, from case packing through conveying to palletizing, can run on a single unified platform rather than a collection of disconnected systems.
The conversations at the show reinforced what many packaging manufacturers already sense: coordinating multiple vendors across equipment with different technology stacks and integration approaches creates delays, cost overruns, and operational complexity that manufacturing teams can no longer afford. Those that need to move quickly to address SKU proliferation and labor constraints need a faster and more efficient route to automation.
![]()
The Vention Experience Bar tied the full picture together. Visitors could move through the stages of design, programming, simulation, and operation within a single environment, seeing firsthand how the same platform that runs the machines also supports every step from initial configuration to day-to-day operations.
What resonated most with visitors was how a platform approach changes the operational equation. When hardware, controls, and software share a common architecture across the line, operators can manage changeovers directly, performance data stays consistent, and support does not require waiting for an integrator to arrive on site.
Where to See Vention Next: Automate 2026
The end-of-line packaging story continues at Automate 2026 in Chicago.
Join Vention at Booth 2828 from June 22–25 at McCormick Place, where you can experience live demos of Vention’s latest software stack and advancements in Physical AI. Explore the Rapid Operator AI, Overhead Range Extender for welding, structural solutions, and the Next Generation Rapid Series Palletizer with fully integrated conveyors.
Whether you are new to Vention or a long-time partner, come see how the platform has evolved and what it can do for your operations.
When: June 22–25, 2026
Where: McCormick Place, Chicago — Booth 2828
Register with code: 119663