Back to blog

Top Five Ways Vention Made Automating More Accessible in Q1

March 28, 2025 | Vention Official

Consistent wood finishing, a more productive weld line, and a smarter approach to machine tending—2025 is shaping up to be a breakthrough year for manufacturing automation. Whether you’re tackling labor shortages or scaling up operations, Vention’s ‘click-and-customize’ approach is making deployment faster and easier than ever. And with the launch of AI-powered bin picking, this is set to be the year of ‘physical AI,’ tackling real-world challenges head-on, without the need for complex programming.

Discover how Vention’s latest solutions are helping manufacturers get more done with less effort.

Five New Automation Solutions from Vention


1. Turnkey Robotic Sanding

With human error accounting for 80% of the manufacturing errors, quality is the top concern for the woodworking industry. Vention launched a turnkey automated sanding solution in collaboration with 3M to address the quality and labor shortage challenges of the industry. This versatile robotic sanding solution allows woodworkers to rapidly automate with no programming knowledge required. The intuitive interface allows you to create sanding recipes and adjust parameters to align perfectly with your current process, making it the easiest way to finish more doors per day.

Learn More About Robotic Sanding



2. Click and Customize Modular Robotic Welding

The welding industry is facing ongoing labor shortages and traditional automation solutions have been expensive, inflexible, and hard to deploy. Vention launched a fully modular robotic welding solution in Q1 to let manufacturers easily build, deploy, and adapt robotic welding cells to their specific needs.

Users can get all necessary components from a single platform to tailor the system to their shop floor requirements with unmatched flexibility. The best part about the click-and-customize solution is that it can be easily scaled up or diversified in response to market demands. The ‘Quick Start’ templates provide a solid foundation for designing a custom welding cell, accelerating implementation and making welding automation more accessible.

Discover Modular Robotic Welding



3. Click and Customize Robotic Machine Tending

Traditionally, automating machine tending required manufacturers to choose between a custom but costly solution, or turnkey but restricted system. Vention introduced a new approach in Q1 2025, combining the flexibility of customization with the speed of pre-engineered solutions. This innovative robotic machine tending solution can be deployed in just two weeks, making it both fast and easy to automate CNC machining.

Explore Robotic Machine Tending



4. AI-powered Bin Picking: Turning Robots Into Autonomous Operators

AI is evolving at an unprecedented pace, making it possible to develop intelligent and precise automation - such as Vention’s new AI-powered Bin Picking solution.

The solution showcased during a live demo at 2025 NVIDIA GTC enables robots to detect, select, pick and organize parts - straight from a CAD file. Powered by Vention’s MachineMotion AI controller, accelerated by NVIDIA Jetson, the intelligent system can turn robots into autonomous, reliable operators.

Learn More About AI at Vention



5. Beyond Boxes – Flexible Palletizing for Any Product

Beyond Boxes

Industries like agriculture, food and beverage, chemicals, construction, and pharmaceuticals hold immense untapped potential for automation but require a solution that can handle unconventional containers. Vention’s flexible palletizing solutions empower manufacturers to seamlessly adapt to products of all shapes, sizes, and weights—from bags to pails and beyond.

Engineered for speed, simplicity, and scalability, it streamlines workflows while ensuring peak performance, making automation more accessible and efficient than ever.

Learn More About Automated Palletizing



Resources to Help You Automate


The Vention team engaged with manufacturers across industries and at all stages of automation adoption with virtual events in Q1. Missed our webinars? You can still watch them here.

  • Vention x ABB: Digitize and Deploy Custom Automation Projects in Days
    Watch now

  • Automated Sanding: High-Quality Results Within Reach
    Watch now

  • End-of-Line Automation 101: How to Get Started, Scale, and Maximize ROI
    Register to watch on-demand



Follow Us to Get the Latest from Vention

That’s a wrap on Q1! You can also get the latest updates about our product launches and events by following us on LinkedIn. Stay tuned for more from Vention soon!

Back to blog