The case for investing in R&D and manufacturing automation has strengthened following the tax cuts introduced under the One Big Beautiful Bill (OBBBA) in the US. Signed into law in July 2025, the bill incentivizes domestic research and enables immediate deductions for select capital investments. For example, Amazon reportedly reduced its tax burden to $1.2 billion from $9 billion the previous year, according to The Wall Street Journal.
For manufacturers navigating economic uncertainty and persistent labor constraints, the timing of this new tax regime is particularly advantageous. Several provisions of the OBBBA materially improve the economics of capital investment in equipment, facilities, and R&D.
Understanding these incentives can support more informed capital allocation decisions for organizations planning automation initiatives. This article outlines the key provisions of the OBBBA, clarifies specific deduction limits, and explains how manufacturers can incorporate these incentives into an effective automation strategy.
Note: This article is for general informational purposes only. Tax treatment varies by business and state, so manufacturers should consult their tax and finance advisors when applying these provisions.
How the OBBBA Helps Manufacturers
At its core, the OBBBA reduces the cost of investing in productivity-enhancing assets by allowing manufacturers to recover capital costs faster through the tax code. The bill restores and expands provisions that encourage capital investment. For manufacturers, the most relevant changes are enhanced expensing and permanent bonus depreciation. Together, these measures improve cash flow, reduce upfront tax burden, and strengthen the returns on automation investments.
Key Provisions
100% Bonus Depreciation Returns
One of the most impactful changes is the restoration and permanent extension of 100% bonus depreciation on qualifying assets placed into service after January 19, 2025. Under this provision, companies can deduct the full cost of qualified equipment in the year it is placed in service rather than depreciating it over several years. While this applies for federal tax purposes, state conformity varies and should be evaluated separately.
Qualified property typically includes:
- Machinery
- Automated equipment
- Robots
- Other tangible assets with a useful life of 20 years or less.
Why this matters:
For automation-heavy manufacturers, bonus depreciation can significantly improve first-year cash flow. Because there is no maximum dollar cap, large robotics or production expansion projects may generate meaningful deductions immediately, strengthening project ROI and shortening payback timelines.
For example, a manufacturer that invests $5 million in automation equipment in 2026 can deduct the entire $5 million on that year’s federal tax return, lowering taxable income and improving cash flow.
Calculate Your Own Deduction Here » https://equipmentfinance.amerisbank.com/section-179-calculator/
Enhanced Section 179 Expensing
Section 179 allows businesses to expense qualifying property rather than depreciate it incrementally. The OBBBA increased the annual deduction limits effective for tax years beginning after 2024:
- Maximum Deduction: Approximately $2,560,000.
- Phase-out Threshold: Approximately $4,090,000.
- Spending Cap: The deduction is completely eliminated once total qualifying equipment purchases reach $6.65 million.
Previously, manufacturers could expense much of their equipment using bonus depreciation, but certain assets, such as software or qualifying building improvements, were often depreciated over several years. With the expanded Section 179 limits, those investments can now be deducted upfront, allowing manufacturers to recover more of their capital immediately and improve early-year cash flow. The result is lower after-tax cost and faster payback, making automation projects easier to approve and scale.
Production Facility Expensing
Beyond machinery and equipment, the OBBBA extends first-year expensing to certain manufacturing facilities through a new category called qualified production property. For projects that break ground after January 19, 2025 and are placed in service before 2031, portions of production buildings can be deducted upfront rather than depreciated over decades.
This provision is particularly relevant for manufacturers making large-scale investments tied to automation-driven growth, such as:
- New production halls or plant expansions
- Facility upgrades required to support robotics deployment
- Specialized buildouts for automated lines, material flow, or advanced manufacturing processes
By treating qualifying facility investments more like equipment for tax purposes, this provision materially improves capital efficiency and accelerates returns on large-scale plant upgrades and automation-led expansions.
Immediate Expensing of R&D
The OBBBA also restores immediate expensing for domestic research and development costs rather than requiring capitalization and amortization over multiple years. For manufacturers investing in automation integration, process optimization, or internal innovation, this change means R&D expenditures can generate an immediate tax deduction in the year they occur.
OBBBA Impact on Automation Economics
Together, 100% bonus depreciation, expanded Section 179 limits, qualified production property expensing, and immediate R&D deductions materially improve the near-term economics of automation investments. By accelerating deductions into the year equipment is placed into service, manufacturers may reduce taxable income, strengthen first-year cash flow, and shorten payback periods for robotics and plant modernization projects.
In practice, these incentives lower the effective cost of capital and make automation business cases more compelling at the executive level. It’s important to also consider the timing. Many benefits depend on when assets are placed into service, meaning deployment schedules can directly affect how much value is captured. Manufacturers should align automation roadmaps with finance and tax teams to ensure projects are structured and executed within the applicable windows.
Aligning Tax Strategy With Automation Targets
Leading manufacturers are increasingly tying automation programs to economically relevant targets that resonate with executive leadership and the board. These targets are typically defined at a top-down level, such as return on capital, operating expense reduction, or measurable throughput improvement.
When OBBBA incentives are applied within this framework, automation projects can deliver stronger financial outcomes and a clearer investment narrative for CFOs and enterprise leadership. Capital plans that account for both operational impact and tax efficiency are generally more compelling and more likely to secure approval.
Four Steps to Identify the Right Capital Investments
Tax incentives like those in the OBBBA create a window of opportunity for manufacturers to accelerate strategic automation investments. To translate this into action, manufacturers should:
- Define automation transformation goals in economic terms
- Align project timeline with tax deduction eligibility
- Update ROI models to incorporate OBBBA benefits
- Evaluate automation platforms that support rapid deployment and scaling
Understanding how these tax provisions affect capital investment and automation economics allows enterprise manufacturers to make better-informed decisions and strengthen their competitive position. For manufacturers who have been on the fence about automation, now is the time to move forward with your plans.
***
Learn more about setting realistic automation targets and aligning a roadmap for automation transformation.