Back to blog

Aluminum Extrusion Systems

May 26, 2025 | Philip Hegarty

Extruded Aluminum Systems: The Backbone of Modern Manufacturing

Extrusion Aluminum System by Vention

Understanding T-Slot Aluminum Extrusion Framing Assemblies

The dynamic manufacturing landscape requires companies to evolve to survive in today’s market and thrive in the future, with many turning to modular solutions like aluminum extrusion framing. Bespoke pieces of industrial equipment that require large capital outlays struggle in facilities that need the flexibility to quickly and efficiently adapt to dynamic demands. From safety fencing and workstations to conveyor systems and adding an overhead 7th axis to a cobot arm, extruded aluminum systems, also called 8020 aluminum extrusions or t-slot aluminum extrusions, offer unprecedented modularity, allowing manufacturers of all sizes to create structural solutions that are versatile and easy to implement.

What is Aluminum Extrusion Framing?

T-slot aluminum extrusion systems are systems for the creation of flexible, modular machine or industrial structural framing. T-shaped slots run the length of the aluminum sections to allow for quick yet secure connections. Together with fasteners, plates, and accessories, aluminum extrusions create a flexible, strong manufacturing framework that can be easily assembled, modified, and expanded. Unlike traditional welded or bolted steel structures, t-slot aluminum extrusion framing provides a lightweight solution that can be rapidly reconfigured to meet changing manufacturing and design requirements.

How Do Extruded Aluminum Systems Work?

Aluminum framing is created through a precision extrusion process. Aluminum billets are heated and forced through a specially designed die under high pressure that creates precision-engineered t-slot profiles spanning the length of each section. The resulting extruded frames are lightweight, durable, and modular. Each aluminum extrusion profile, named based on its dimensions, is a modular building block that can create complex structural systems with minimal additional fabrication.

The Structure of Aluminum Extrusion Framing

Modular extruded aluminum profiles come in various shapes and sizes. The main feature of aluminum extrusion framing is its unique channel design that ranges from simple grooves to complex, multi-slot configurations that offer increased flexibility.

These are the common components of extruded aluminum framing:

Profiles

The profile is the backbone of the modular aluminum framing system. 8020 aluminum extrusion is available in different weights and footprints based on your use case and budget. Extruded aluminum profiles range from lightweight and compact options to profiles engineered for extreme industrial environments that support cobot arms or conveyor systems and require maximum rigidity and minimal deflection.
Vention’s extrusion profiles are optimized for best-in-class ratios of the moment of inertia per unit of surface area. Learn how we’ve optimized high-performance assemblies with innovative t-slot profiles that improve tolerances and strength-to-weight ratios.

Interface

T-slot channels run continuously along the aluminum extrusion profile, creating an interface of versatile connection points for easy customization and continual updating throughout the equipment’s lifecycle. T-nuts and fasteners slide into the profile’s t-slots, allowing for tool-free, adjustable connections. Fasteners, brackets, and accessories can be positioned anywhere along the slot, enabling infinite configurability and precise alignment, and can all be attached without drilling, welding, or otherwise altering the profile.
The interface channels are engineered for weight and function and enable multi-axis connections to greatly simplify assembly and future changes. Vention’s patented V-shaped interface provides increased rigidity and precision. The self-aligning joints support up to 25% more payload than traditional assembly plates and aluminum extrusion profiles and the double-arm design redistributes material from the profile’s center towards the outside, increasing strength and stiffness while reducing overall material and, thus, weight.

Fasteners

Fasteners are the mechanical components that join profiles together and attach accessories to the extruded aluminum framing. This connection hardware provides structural integrity to the frame and allows for quick repositioning and removal. Some fasteners are external and some internal, while some are designed for strength and others prioritize features like accessibility. Examples include t-nuts, screws, angle brackets, joining plates, and end connectors.


Mechanical Specifications of Aluminum Extrusions

Understanding the mechanical specifications of extruded aluminum profiles is crucial, especially when designing t-slot aluminum extrusion structural applications. Properties a buyer should consider include:

Area moment of inertia

Area moment of inertia (or the second moment of area) describes an extruded aluminum profile’s resistance to beam bending. A higher value indicates greater resistance to deflection or bending under load. This is essential for applications like machine frames, gantries, or vertical supports where stiffness and stability are critical. For non-square extrusion profiles, the moment of inertia will depend on the extrusion’s orientation.
Vention’s aluminum extrusion profiles offer an industry-leading area moment of inertia that enables highly rigid structures.

Cross-Sectional Area

An extruded aluminum profile’s cross-sectional area is the total area of the profile’s cross-section, measured in square millimeters or inches, which directly relates to its overall strength and weight. A larger area generally means more material to resist axial forces (compression/tension) but also increases weight and cost. For vertical supports or tension members, more area means more load-bearing capacity.

Torsional Constant

Torsional Constant (J) is the measure of a profile’s resistance to twisting (torsion) along its axis. This is crucial in applications like robotic arm bases, extended cantilevers, or XYZ gantry framing where the structure is subjected to rotational forces.

Real Extrusion Picture

Yield Strength

Yield Strength is the stress level at which the aluminum permanently deforms. Beyond this point, the profile won’t return to its original shape, indicating the maximum safe load the material can handle without failing. It’s the ultimate threshold for structural integrity and is critical in safety-sensitive or high-load environments.


What is Aluminum Extrusion Framing Used For?

The flexibility of extruded aluminum framing makes it versatile for use across various industries. Easy to disassemble and reassemble into new configurations with interchangeable system components, aluminum extrusion frameworks are ideal in facilities where products or processes often change or where there are frequent setups and teardowns. From test rigs to machine guardrails, conveyor systems, and storage solutions, modular aluminum framing is commonly used in these industrial applications:

Industrial Automation

Industrial Automation
Today’s aluminum extrusion profiles are reliable, rigid, and industrial-grade components suited for a wide variety of automation applications. T-slot profiles are commonly used with robotic systems in manufacturing facilities, and modular aluminum framing is used to design robust, lightweight frames for collaborative robot arms and conveyor equipment.

Safety Enclosures and Machine Guarding

Safety Enclosure
Extruded aluminum profiles enable quick construction and modular reconfiguration of strong, lightweight safety enclosures and workstations that can be quickly redesigned to efficiently adapt to changing production needs. Extruded aluminum safety enclosures can be easily implemented in fenced, fenceless, or hybrid arrangements.

Industrial Logistics

With aluminum structural framing, companies can construct material handling systems, storage solutions, and transport frames that adapt to changing warehouse and logistics requirements.

Ergonomic Workstations

Ergonomic Workstations

Companies can easily build custom fixed or mobile workstations, carts, shelving, and storage systems with aluminum extrusion framing. Modular solutions create a lean and collaborative work environment that can be quickly modified to help efficiently optimize production processes while ensuring worker safety and comfort are prioritized.

Research and Development

Engineering and R&D teams use aluminum extrusion framing to build enclosed cells, experimental setups, test rigs, and prototype structures that can be quickly adjusted without extensive fabrication.


Benefits of Extruded Aluminum Framing

The benefits of t-slot framing range from design flexibility and modularity for evolving needs to take advantage of the material performance, high strength, and light weight of aluminum.

Aluminum Extrusion Advantages

Aluminum is about one-third the weight of steel. When extruded into t-slot profiles, lightweight aluminum framing unlocks a powerful combination of versatility, strength, and efficiency that transforms how industrial structures are designed and implemented.

Modularity Advantage of Aluminum Extrusion Frameworks

Extruded aluminum framing systems are faster and less costly to assemble than traditional welded steel structures. The t-slot designs of aluminum extrusions allow for quick connections, making it simple for facilities to implement, optimize, and expand production setups. Modular aluminum framing enables future expansion without a major rebuild, specialized labor, or large capital investment. Manufacturers eliminate the need for complex fabrication by simply loosening and repositioning fasteners or adding and subtracting frames to modify production lines.

Operational Efficiency

Productivity begins with safety and efficiency, and modular aluminum extrusion framing allows companies to quickly create lean production lines and ergonomic workstations as well as optimize based on operational experience or market demands. 
The modularity of 8020 aluminum enables easy customization for your facility’s layout – creating safer workspaces with easy-to-build protective structures that improve worker safety or eliminating non-value-added steps that help minimize waste and reduce cycle times. 
Simple setup and adjustments also mean reduced downtimes for implementation and retooling – creating a strategic advantage out of your team’s imagination combined with the easily reconfigurable industrial design of extruded aluminum framing.

Strength-to-Weight and Material Performance of Extruded Aluminum

Aluminum extrusions are lightweight and easy to handle. Extruded aluminum profiles are strong enough to support heavy loads without bending or breaking and are corrosion-resistant, making them ideal for service even in wet or corrosive industrial environments. 
Compared to square tubing, the t-slot groove on the face of extruded aluminum framing lowers its rigidity. This has led to some misconceptions that aluminum framing systems cannot meet the demands of factory environments where welded steel is the norm. However, recent advances, including from our engineering taskforce, have led to stronger and more vibration-resistant frames with higher capacities. Vention’s high-precision extrusions rank best-in-class in terms of structural rigidity and Vention’s XL extrusions are the first modular extrusion kit specifically designed for the next generation of heavy-duty cobots.

Cost Effective

Minimizing costs is essential for business optimization. Using standardized extruded aluminum components and accessories simplifies implementation and reduces the need for custom parts or extensive design work. Aluminum extrusion framing offers long-term savings because it’s durable and modular, reducing the need for frequent replacement parts while also being significantly lighter than steel, lowering shipping costs and making handling safer and easier.

With strength performance comparable to steel, using extruded aluminum framing allows companies to eliminate implementation tasks like welding, coating, or painting, making extruded aluminum the more cost- and time-effective solution for industrial framing projects.


Aluminum Extrusion Cost: How Much Does Extruded Aluminum Framing Cost?

The price of a t-slot modular aluminum framing project depends on multiple factors, but typically delivers exceptional return on investment through labor savings, adaptability, and reusability.

Initial costs depend on variables like the size and complexity of your layout, as well as the load requirements that drive the profile size decisions. Larger or reinforced profiles or additional connection components impact overall system costs. Comparing extruded aluminum framing lengths of approximately 6ft (1845mm), 45x45mm t-slot profiles start around $60, while 247.5x247.5mm XL extrusions with their double-walled design cost about $1,100 per section. Frame connectors and assembly plates generally cost under $50, whereas accessories like panel sliding doors can be added for a few hundred dollars.

Using aluminum extrusion framing can also help manufacturers minimize long-term maintenance costs. T-slot aluminum extrusions often use bolt-together connections, eliminating the need for welding and reducing skilled labor costs. On-site adjustments are easy to implement, saving costs for replacement parts, labor, and machine downtime time during installations and retrofits.


Showcase of Modular Aluminum Framing Success Stories

Framing Ergonomics Empower Small Business

PMB Suspension, a Swiss-based mountain bike suspension specialist, needed a cost-effective, ergonomic solution to enhance productivity in its workshop. Vention delivered seven custom-configured carts, workbenches, and jigs. Configured from Vention 45x45mm aluminum extrusions, the entire setup was shipped within a week and fully assembled in under a day. The modular design improved workflow efficiency and provided an aesthetically pleasing environment for visiting customers. As a result, PMB Suspension achieved the same revenue as shops with teams four times larger, all while maintaining a lean operation. Read the full story about rapid deployment aluminum extrusion framing.


Rapid Response Manufacturing with Modular Aluminum Framing

A manufacturer automating local operations to stay competitive in response to a large surgical mask order required safety enclosures around the robotic cells. Guarding constructed of extruded aluminum framing easily added the operational safety to meet North American and International standards. Safety interlock switches provide quick access for workers if an intervention is needed on the equipment. Partnering with Vention, the project, from design to commission, was completed in just five days. Learn more about the extruded aluminum safety enclosure for a robotic surgical mask machine.


Aluminum Extrusion Innovation Unit for Complex Shade Testing

Legrand, a designer and manufacturer of manual and automated roller shade solutions, partnered with Vention to develop a custom testing fixture that could accommodate various product sizes and configurations. The project demanded a robust and adaptable solution capable of supporting complex testing procedures while allowing for easy modifications. Leveraging Vention’s modular aluminum framing system, Legrand engineered a flexible and safe structure capable of mounting multiple shades with varying heights and sizes at once while also quickly reconfiguring to serve different customers. See how Legrand built its modular aluminum framing solution to minimize footprint and maximize available space.


Doubling Cobot Productivity with an Extruded Aluminum Overhead 7th Axis

WALT Machine partnered with Vention to automate the tending of three CNC lathes using a single UR10 collaborative robot. To meet the demands of an important production contract, a 40-foot overhead 7th-axis range extender was needed to enable the cobot robot to service all the machines efficiently. Deploying an extruded aluminum framework configuration helped double production output, and partnering with Venton reduced deployment time from three months to three weeks. Learn more about achieving 5x the cost savings compared to the traditional approach.


How to Choose the Right Modular Aluminum Framing System

Extruded aluminum can be used in a variety of industrial settings – from light-duty profiles creating enclosures and guards, while medium-duty profiles serve as machine or cobot pedestal bases, carts, and workstations. Heavy-duty options, like Vention’s XL extrusions, are specifically designed for high-load applications like gantries and automation cells with next-generation cobot robots. Evaluating the right factors before investing in an 8020 aluminum extrusion framing system ensures alignment with operational goals, budget, and growth trajectory.

How to Choose Modular Extrusion Systems

Factors to Selecting Extruded Aluminum Systems

Calculate the Safety Factor for Load and Structural Requirements

As with any successful project, implementing 8020 framing begins by thoroughly analyzing your design, load characteristics, and workflow needs. Your profile should be determined by the scale and strength needed for your project. Develop specifications for the appropriate framing system based on your payload, precision, and flexibility requirements.

Understand the maximum weight and force requirements, including any additional loads from mounted components. You must always calculate the force at failure over the allowable load to add an adequate safety factor (SF). For example, if a structure will theoretically fail at 1000 N of force, a safety factor of two would establish an allowable load limit of 500 N. Determine your safety factor according to your industry’s standards (a safety factor of 4-5 is suggested) and always increase the safety factor if there is any risk of injury occurring due to system failure.
Safety factors should be based on, but not limited to, variables like calculation accuracy and thoroughness, environmental conditions, consequences of failure, and the cost of overbuilding. Vention’s t-slot aluminum extrusion deflection calculator helps you easily determine stress, deflection, and safety factors.


Choose the Right Aluminum Extrusion Profile

To choose the right extruded aluminum profile for your application, balance the tradeoffs between strength and material efficiency, especially in mobile cobot or weight-sensitive extruded aluminum designs. Remember, not all aluminum extrusion profiles are created equally. Even if two profiles have the same outer dimensions, 45 x 45 mm, for example, their rigidity may vary significantly depending on their area moment of inertia. Choose profiles with a high moment of inertia for long spans or heavily loaded beams.

Also, the cross-sectional area, which affects the overall weight of the assembly, should be considered. Since the best profiles are highly rigid and lightweight, a top performance indicator is the area moment of inertia to surface area ratio.

Some suppliers may require you to stick to one profile series for connections. Vention, on the other hand, offers uniform fasteners and assembly plate hardware, making profiles of various sizes compatible to ensure you can create an assembly optimized for strength and efficiency.

Use the Right Fasteners for Load and Access

Combining effective assembly joints with the appropriate extrusion profile can improve the structural integrity of your framework, so it’s important to invest in the proper connection components for your t-slot framing. Choose connection methods based on structural demands, access requirements, and ease of assembly. For high-load applications, prioritize corner brackets, gussets, or tension plates over standard joining plates. Use internal fasteners like hidden corner connectors for clean aesthetics and strong joints. Choose quick-connect fasteners or clamping mechanisms for areas requiring frequent adjustments or modularity.

Ensure the fastener size matches your profile, or stick with Vention aluminum extrusion products that feature a uniform fastener size across all profiles to guarantee maximum flexibility. Always torque fasteners to spec and use anti-vibration products like spring washers or locking T-nuts in dynamic environments to prevent loosening over time.

Plan with a CAD Library

Simplify your design process and ensure component compatibility with a CAD model. Vention’s MachineBuilder tool helps manufacturers navigate from idea to finalized design in minutes with drag & drop components, AI-driven part recommendations, a configuration assistant, and a smart design checker. Vention also offers design templates to jumpstart your project and a comprehensive selection of structural aluminum profiles and fasteners in our online store of plug-and-play components.  If the freedom of modularity is too intimidating or your project is too complex, connect with a Vention expert to get help designing your project.

Plan with a CAD Library

Evaluate Extrusion Accessories and Compatibility

When choosing a system, prioritize compatibility across profile sizes and check for a robust ecosystem of accessories: cable management, enclosures, motion components, and robot arms. Vention’s platform, for example, is built for scale and integration, from structural framing to motion and control, while maintaining consistent hardware interfaces across all profile sizes. This allows you to prototype quickly and confidently expand without starting from scratch. A well-supported ecosystem ensures your framing system can grow with you as your manufacturing needs evolve.


How to Implement Extruded Aluminum Framing

Extruded aluminum framing systems like t-slot profiles offer versatile framework solutions for industrial and manufacturing applications that combine strength, lightweight construction, and adaptability. These systems can significantly reduce design time, assembly costs, and maintenance requirements. The following tips will help you maximize your extruded aluminum framing investment’s value, structural integrity, and versatility.

Best Practices for T-Slot Framing Implementation

Maximize the value of your extruded aluminum framing investment with these considerations and best practices.

Rightsize Extruded Aluminum for Your Project

Choose a profile series and connection components with appropriate safety margins and structural integrity for your needs but the smallest profile that safely handles your load to optimize your investment. Seek a balance of strength and weight without overbuilding, as oversized profiles increase weight and cost with little benefit. For example, save weight and expense by using reinforced joints only where needed under heavy loads and long spans or by switching to a lighter profile where appropriate. Using an extruded aluminum product with compatibility across different profile sizes helps manufacturers optimize their projects.

Extruded aluminum profiles are available cut to a variety of sizes. Use standard lengths where possible to reduce waste and cost.

Design Effective Assembly Joints

Combining effective assembly joints with the appropriate extrusion profile can improve the structural integrity of your assemblies. Joint configuration can substantially change the rigidity of a design. For example, it’s best practice to avoid relying on friction-based joints to support the load. Try the Vention Friction Joint Calculator to determine the load capacity of a joint fixed in place by pure friction.

Calculating the necessary assembly plate size is also an excellent way to optimize the cost of your design. It’s tempting to choose the strongest assembly plate available, but you can save costs on extruded aluminum frameworks by going with one that only fits the number of fasteners needed and no more. Vention connection plates come in GP (general purpose) and HP (high precision) variants, giving manufacturers choices to optimize for lower price or higher strength and precision.

Check out our extruded aluminum design guide to learn more about designing with t-slot aluminum extrusions.

Maintain Squareness and Tolerance

Precision matters – especially when building automated systems, enclosures, or robot bases. Even small misalignments can introduce stress, vibration, or tracking errors in motion systems. Use levels and calibrated squares during assembly and tighten fasteners in sequence to avoid warping.

Vention simplifies this process by offering self-aligning extrusion connections and a line of XL aluminum extrusions designed specifically for the next generation of heavy payload cobots that feature a floor anchoring plate with built-in leveling features and smart assembly plates to ensure perfect alignment.


Integrate Cable Management from the Start

Use a cable management system for cable routing as part of your structural design to improve safety, aesthetics, and serviceability. Use internal channels, covers, and snap-in profiles to cleanly manage cables and pneumatic lines. Design pathways that minimize cable movement and fatigue, especially in dynamic applications with motion. Leave clearance in profiles for zip ties, drag chains, or cable clamps to reduce wear and prevent interference with moving parts. Learn more about cable management equipment here.

Cable Management

Design for Modularity and Expansion

8020 aluminum systems are inherently flexible, but make sure you’re getting the most out of your investment by choosing products that feature uniform mounting hardware so profiles of various sizes can be combined together to create custom assemblies.

Evaluate if or how easily the aluminum framing adapts to new designs once implemented in order to integrate with future manufacturing needs. Designing subassemblies that can be independently built, tested, and upgraded is best practice, but only if they can easily integrate into your modular aluminum framing ecosystem.

Leave room in the design for future mounting, wiring, or upgrades. Use sliding t-nuts that allow components to be added without full disassembly. Plan for reusability by avoiding permanent modifications like welding or glue. Cap off open ends to keep profiles clean and avoid debris buildup.


Unlimited Customization Possibilities with T-Slot Aluminum Framing

Every application in every facility is unique, requiring tailored solutions to meet its specific operational needs. T-slot aluminum framing allows companies to increase design flexibility, reduce fabrication time, and create more cost-effective and adaptable industrial solutions. Construction and modifications with traditional welded steel framing requires labor- and time-intensive cutting, welding, priming, and painting. However, quick-ship extruded aluminum framing makes creating safer, more productive, and cost-effective workspaces achievable at any scale to support both immediate productivity and long-term growth goals.


Whether you’re designing a simple workstation, implementing complex automation infrastructure, or futureproofing your entire production facility, 8020 aluminum extrusion framing provides the foundation for manufacturing excellence in an increasingly dynamic marketplace.

Back to blog