Tools
Checklists
Factory Acceptance Test Checklist
The checklist tool for Factory Acceptance Tests assists you in setting clear expectations for machine functionality and allows you to validate these were met prior to shipment from the factory. Download your FAT checklist to validate your next project.
Site Acceptance Test Checklist
The checklist tool for Site Acceptance Tests assists you in setting clear expectations for deploying machines into production on-site at your facility, and allows you to validate that all systems are operational in accordance with the functional specifications. Download your SAT checklist to deploy your next project.
Calculators
Deflection Calculator
Determine the strength, maximum deflection, and safety factor of a simply supported or cantilever extrusion beam. This will verify the load supported by a horizontal beam, and if the beam is rigid enough for the application.
ROI Calculator
Quickly calculate the return on investment for your next automated equipment project. Define parameters for the process you seek to automate and get results in terms of production volume and months required to breakeven and payback your investment.
Friction Joint Calculator
Many joints made with extrusions rely on pure friction. Determine the load capacity of a pure friction joint by specifying the installation torque of the bolts and the number of fasteners.
Application Configurators
Pallet Configurator
Create pallet configurations by defining box sizes and pallet types, then use auto-layout and auto-stack to optimize your configuration. There are also advanced features for creating exact layouts when needed. The configurations are used as programs for Vention's Palletizers.
Path Following Configurator
Create path patterns by defining your workspace, mapping your axes and outputs, and configuring your path sequence. Then visualize your path and perform a dry run at an offset from your working piece to ensure proper operation. There are also advanced features that help you simulate your entire process before deploying to the machine. The configurations are used as programs for Vention's path following turnkey applications.